E Path logo

Türk Prysmian Kablo promotes eco-friendly cable production with the E-Path label

categories: Corporate 

Carbon footprint decreases and efficiency increases

16/10/2024 - 10:00 AM

Türk Prysmian Kablo, the world's leading energy and telecom cable company, aims to reduce carbon emissions by providing environmentally friendly solutions in manufacturing cables. Türk Prysmian Kablo, which eliminates the use of toxic substances with its E Path label and prefers recyclable materials, minimizes the loss of energy thanks to its high transmission efficiency. 

Türk Prysmian Kablo continues to develop sustainable solutions to the problem of carbon emissions, which have reached serious proportions with the rapid growth of cable production. Türk Prysmian Kablo stands behind its commitment to sustainability, reliability and quality by promoting environmentally friendly production processes with the E Path label. Türk Prysmian Kablo is committed to protecting both human health and the environment by avoiding the use of toxic substances and preferring recyclable materials following REACH and RoHS regulations. It aims to contribute to raising environmental awareness in the sector by minimizing energy lost due to its high transmitting efficiency. 

Designed to comply with the Eco-Labeling Regulation 

The E-Path label was developed based on sustainability, reliability and quality in accordance with the European Union's Ecolabel regulation. Türk Prysmian Kablo's products bearing this label are among the first in the cable industry to be awarded the green label. The aim of E Path is not only to create environmental awareness but also to set a new standard for the sector. 

It is evaluated on the basis of 6 criteria 

A cable must meet several criteria to receive the E-Path label. Cables that carry this label are evaluated according to six criteria: carbon footprint, recyclability, recycling input rate, non-use of toxic substances, environmental benefits and transmission efficiency. All stages, from cable production to recycling processes, are carefully examined. Emissions throughout the product life cycle are calculated in accordance with the ISO 14067:2018 standard to minimize the impact of climate change.

It attaches great importance to its products' environmentally friendly production and recycling.

Acting in accordance with the REACH and RoHS regulations to prevent the use of toxic substances, Türk Prysmian Kablo does not allow the use of substances that are carcinogenic and harmful to the environment in its cables. It also makes sure that the materials used in manufacturing its cables are recyclable by focusing on recycling processes. This approach contributes to the efficient use of natural resources and minimizes waste generation by encouraging the use of 10% recycled materials. The E Path label symbolizes this sustainable production approach.