Prysmian Group in Türkiye

Overview

Turkish operation of a worldwide leading company, Prysmian.

With almost 150 years of experience, 30,000 employees and 108 factories in more than 50 countries worldwide, it has focused on high-tech markets.

 

Türk Prysmian Kablo ve Sistemleri A.Ş. is Turkish operation of Prysmian, worldwide leading company in energy and telecommunication cables’ industry. The company is headquartered in Mudanya (Bursa) since 1964 and carries out its activities in a total area of 180.000 m² (covered area: 79.000 m²).

Prysmian Türkiye

31st December 2023

experince_icon

60

Years of Experience

countries_icon

%29

Export

ürünlerimiz

+22.000

Different Cable Production

economic_icon

+14B

Sales in TRY

Prysmian Türkiye

The company stands out in Prysmian as one of the 16 plants that can simultaneously produce energy and telecom cables with Prysmian and Draka brands. Wide product range of Türk Prysmian includes all energy cables up to 220 kV, copper conductor communication cables up to 3.600 pairs, optical fiber cables, railway signalization cables, studio broadcast cables and special cables. Today Mudanya factory can produce over 22.000 different cables. Furthermore, Türk Prysmian delivers “turn key” projects for cables and systems providing each one customer tailored and premium services. 

The installed capacity of Türk Prysmian is also at a level to compete in the international markets. Capacity utilization rate of Türk Prysmian reached 71% in 2024, and it continues to be a privileged export center within Prysmian, exporting approximately 29% of its TRY 14.323.612.636 turnover in 2024. Türk Prysmian continues to be the leader of the market in the field of innovation, technology, quality and customer satisfaction both in Türkiye and abroad. With a wide geographical coverage, the company exports to more than 50 countries today, particularly Turkic Republics and Middle East countries.

Prysmian has 26 R&D centers worldwide and one in Türk Prysmian’s Mudanya factory. Material Technologies Laboratory in the Mudanya R&D center is registered by Turkish Accreditation Agency (TÜRKAK) with accreditation certificate TS EN ISO/IEC 17025 “General Requirements For The Competence of Testing and Calibration Laboratories”. The certificate granted by TÜRKAK is a certification that the results of ‘fire tests’ conducted in Türk Prysmian’s laboratory are reliable and internationally valid. 

Türk Prysmian Kablo ve Sistemleri A.Ş., listed on the Borsa Istanbul strives for improving the efficiency of its products and services not only in Türkiye, but also in global markets, and ISO/DQS 9001, and ISO 14000 certifications granted for the first time in this sector is a further proof of how much the company cares for people and environment.

Contact Us


Headquarter - Mudanya/Bursa

Headquarter

Ömerbey Mah. Bursa Asfaltı Cad. No:51 Mudanya 16941 - Bursa