"Attention! All Solar (PV) Cables Are Not the Same..."
Türk Prysmian Kablo addressed five continents at SolarEX Istanbul Türk Prysmian Kablo showcased its sustainable projects and products at the 17th International Solar Energy and Technologies Fair, SolarEX, which hosted investors from over 125 countries. The company highlighted the longevity of its Solar (PV) cables, which exceed 25 years of usage with the project "Attention! All Solar (PV) Cables Are Not the Same...".
The International Solar Energy and Technologies Fair SolarEX, held from April 10-12, 2025, hosted investors from over 125 countries across five continents. At SolarEX Istanbul, the largest International Solar Energy and Technologies Fair in Eurasia, Türk Prysmian Kablo, a global leader in the energy and telecommunication cables sector, introduced its innovative products and technologies with the project " Attention! All Solar (PV) Cables Are Not the Same...".
Preferred in the Turkish market
Türk Prysmian Kablo, leading the sector with its sustainability efforts, introduced the project " Attention! All Solar (PV) Cables Are Not the Same..." at the 17th International Solar Energy and Technologies Fair SolarEX. The project, which is the fourth phase of the initiative " Attention! All Solar (PV) Cables Are Not the Same..." started in 2012, was prepared based on tests and research conducted on Solar (PV) cables. According to the Prysmian Performance Test (PPT) results, Türk Prysmian Kablo's Solar (PV) cables show superior performance and continue to function beyond the standard lifespan of 25 years. Additionally, Türk Prysmian Kablo certifies its Solar (PV) cables with the compliance of reputable testing and certification organizations such as TSE, TÜV, and VDE, and fully compliant products with EN50618 standards are highly preferred in many projects in the Turkish market.