Artificial intelligence and digitalization are increasing the need for sustainable infrastructure in data centers
Prysmian responds to the transformation of data centers with sustainable infrastructure solutions
As artificial intelligence and digitalization gain momentum, driving the growth of data centers, the energy, connectivity and sustainability needs of these infrastructures are also increasing. By strengthening its global expertise in energy and digital transformation, Prysmian is focusing on delivering more comprehensive and sustainable infrastructure solutions for the evolving needs of data centers.
The widespread adoption of artificial intelligence applications, the growth of cloud services and the increasing integration of digital services into everyday life are rapidly increasing data generation and processing capacity worldwide. The physical consequence of this growth is an increasing need for more data centers and stronger digital and energy infrastructure to support them. Rising processing power and data traffic require infrastructure not only to deliver greater capacity, but also to be designed in a reliable, energy-efficient and sustainable manner.
Operating globally in energy and telecommunications infrastructure, Prysmian develops solutions for the evolving needs of data centers through an approach that addresses digital and energy transformation together. By combining its expanding capabilities through new partnerships with its expertise in energy and digital infrastructure, the company aims to offer more comprehensive and sustainable solutions for the future of data centers.
As data centers grow, infrastructure needs are also changing
As artificial intelligence becomes more widespread, the need for infrastructure capable of supporting higher processing power and data traffic in data centers is increasing. This is making energy efficiency, scalability and sustainability just as important as capacity and reliability in data center investments.
A study conducted by Ciena with more than 1,200 telecommunications, fiber operator and service provider professionals across 12 countries also demonstrates the pace of transformation in digital infrastructure. While 90% of respondents expect high-capacity, AI-driven network services to be one of the main sources of revenue growth over the next 3-5 years, 88% see an urgent need to enhance optical networks to meet AI connectivity requirements.
This outlook indicates that not only connectivity capacity, but also the energy infrastructure supporting that capacity, will play a critical role in the future of data centers. Joint planning of data centers and energy systems is becoming increasingly important to sustainably meet rising processing power and data traffic requirements.
Sustainability will shape the future of digital infrastructure
The growth of data centers brings with it increased energy consumption and a greater need for more efficient infrastructure. Therefore, for digital transformation to progress sustainably, it is becoming increasingly important to develop energy infrastructure with reliable, efficient solutions that have a lower environmental impact.
Prysmian considers sustainability one of the core elements of its business model, from the development of its products and technologies to manufacturing processes and infrastructure investments. The company focuses on developing solutions that help reduce energy losses, use resources more efficiently and lower the environmental impact of products throughout their life cycle. In doing so, it aims to contribute to making the growth of data centers and digital infrastructure more sustainable alongside the energy transition.